2019-10-14 7:09 AM
Dear all,
Could not verify ST device!
This error popped up suddenly and blocks any progress. I took an older computer and had the same error again.
Therefore, I suspected a hardware failure and ordered new adapters and processor boards, but I kept having the same error again.
I have upgraded the STM32CubeIDE, the st-link drivers (dpinst_amd64.exe) and st-stlink-server(st-stlink-server.1.1.1-3.msi).
The st_link v2 adapter have been upgraded with the latest firmware.
Using STM32 Link Utility, I was able to program, verify and run blink applications.
I am using BluePills (STM32F103C8) with chinese adapters on a 64 bit Windows 10 machine.
Please find below the output produced when starting debugging in STM2CubeIDE using the GDB server in SWD mode.
I also selected the OPENOCD debugger, but it also failed, though in a different way.(see below)
Does anyone have a suggestion how to proceed on this?
Cheers, Paul
..........................ST-LINK GDB server.....................
STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\Users\Paul_2\Documents\STM32\Workspace\test\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
Hardware watchpoint supported by the target
SWD frequency = 4000 kHz
ST-LINK Firmware version : V2J31S7
Device ID: 0x410
PC: 0xc6640804
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.17 V
Vendor = 0x55
Error in initializing ST-LINK device.
Reason: ST-LINK: Could not verify ST device! Abort connection.
......................OPENOCD.........................................
Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-23-20:37)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only separate srst_nogate srst_open_drain connect_assert_srst
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 8000 kHz
adapter_nsrst_delay: 100
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : clock speed 8000 kHz
Info : STLINK v2 JTAG v31 API v2 SWIM v7 VID 0x0483 PID 0x3748
Info : using stlink api v2
Info : Target voltage: 3.166882
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Stlink adapter speed set to 4000 kHz
Warn : UNEXPECTED idcode: 0x2ba01477
Error: expected 1 of 1: 0x1ba01477
in procedure 'init'
in procedure 'ocd_bouncer'
2019-10-14 11:22 PM
Hi !
I am not very fluent in SWD, but the verbose output from Open OCD helps to identify the issue : the ID read by both tools differs from what is expected. Meaning that the error is the same in both cases.
Your device under test reads back 0x2ba01477 while the tools expect 0x1ba01477. I don't think it can be an electrical problem. Since you are using a bluepill, maybe the microcontroller is a counterfeit product. You should ST about this, perhaps with a picture of the uC.
2019-10-17 4:50 AM
Could not verify ST device!
Thank you so much, Kraal!
I inspected the looks of the chip and found it quite different from the ones I used before.
The text was not engraved but printed in a sloppy way. I think that your suggestion of a counterfeit is right.
I tried to make these counterfeits working under STM32CUBEIDE and OpenOCD.
Therefore, I adapted the st_scripts/target/stm32f1x.cfg file by replacing the 0x1ba01477 by 0x2ba01477.
I also added a line:
reset_config trst_only
This gives a error message:
Error: BUG: can't assert SRST
Neverthless, I could load and debug my code.
2019-10-17 7:27 AM
Hi Paul,
I'm glad you find a way to use your dev board even if the device ID is not correct.
I would add that for test or learning purpose it is OKish to use the bluepill with the strange part as it is, but for anything that goes into production you should always use real product.
Best regards,
Kraal
2020-03-16 1:44 PM
Hi PZwar,
I have the same problem.
However I am unable to locate the "st_scripts/target/stm32f1x.cfg" file or folder on windows 10.
Using STM32CUBEIDE and OpenOCD.
Thanks & regards
=====================Debug log =========================================
Open On-Chip Debugger 0.10.0+dev-01193-g5ce997d (2020-02-20-10:57)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only separate srst_nogate srst_open_drain connect_assert_srst
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 4000 kHz
adapter_nsrst_delay: 100
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : clock speed 4000 kHz
Info : connected to stlink-server
Info : stlink-server API v1, version 1.3.0
Info : STLINK V2J36S7 (API v2) VID:PID 0483:3748
Info : using stlink api v2
Info : Target voltage: 3.180552
Info : SRST line asserted
Warn : UNEXPECTED idcode: 0x2ba01477
Error: expected 1 of 1: 0x1ba01477
2020-03-16 3:41 PM
2020-03-17 9:34 AM
Hey PZwar,
Thanks found it!! :)
I am using STM32CubeIDE_1.3.0, found /stm32f1x.cfg --> path below
"C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.debug.openocd_1.3.0.202002181050\resources\openocd\st_scripts\target"
Got the STM32CubeIDE to download and debug code after doing the chip id changes.
Thanks
2020-03-17 10:29 AM
Hmm the MSB bits of the ID Code register are just a version number so 2 means newer than 1.. ?
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.100230_0002_00_en/Chunk424975896.html
2020-05-15 7:08 PM
If you replace 0x1ba01477 with 0x2ba01477 in stm32f1x.cfg, then it will work for the clone but not for the genuine STM32…
Instead do the following: >>
The zero tells OpenOCD to ignore id numbers, which means all clones or genuine MCUs will work.
Information Source: http://openocd.org/doc/html/TAP-Declaration.html#TAP-Declaration-Commands
2020-05-17 9:07 AM
hey JElli.1,
Thanks for the new info..
I tried it and it works for the clone. 8) :thumbs_up:
But my order for the original is still not delivered thanks to COVID-19.. shall update once i test both.
regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.