2021-06-16 6:27 AM
Hi everyone,
I found this board in the internet and the seller said that this is a new revision of the STM32F4DISCOVERY board. Is it true or not ?
Thank you all.
Solved! Go to Solution.
2021-06-16 7:41 AM
New versions of several boards are blue, WaveShare is also an OEM manufacturer, as I understand the situation.
You colleague should focus on the issue, unlikely to be with the fact the board is blue. Double check if newer components have been used for some of the sensor parts, and if appropriate defines are set in the build to deal with specific board revs where differences may be present. Check README.TXT files in current CubeF4 example projects.
2021-06-16 7:12 AM
Hello @DTran.3 and welcome to the Community :)
The new order code is STM32F407G-DISC1 Discovery kit with STM32F407VG MCU (replaces STM32F4DISCOVERY kit).
Imen
2021-06-16 7:17 AM
Hi Imen,
I just want to now if the blue board is genuine or it's a re-make version of the STM32F407G-DISC1. My colleague now is confusing with a problem with a blue board, so if the board is not genuine I think that it's the main reason of his problem.
Thank you.
2021-06-16 7:41 AM
New versions of several boards are blue, WaveShare is also an OEM manufacturer, as I understand the situation.
You colleague should focus on the issue, unlikely to be with the fact the board is blue. Double check if newer components have been used for some of the sensor parts, and if appropriate defines are set in the build to deal with specific board revs where differences may be present. Check README.TXT files in current CubeF4 example projects.
2021-06-16 7:43 AM
>> Is it true or not ?
TRUE, there are some NEW revisions of the F407, F429 and F746 DISCO boards which are definitely BLUE
2021-06-16 8:56 AM
Thank you so much :)
2021-06-16 8:56 AM
Thank you so much :) again :D
2021-06-17 1:01 AM
Hi @DTran.3 ,
Sorry for the late reply on this, as I am very busy this period with other tasks.
I cannot give all the details based on a simple internet screenshot that can be copied anytime/anywhere.
Nevertheless, I can confirm that new version of STM32F407G-DISC1 is now assembled with PCB in blue color.
I clearly seen an additional sticker on the top of insert card that was recently introduced in manufacturing process, describing bar code, FG, CPN and batch information.
In conclusion, the blue board is the new version and all new DISCOVERY boards family will adopt this PCB color.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.