2021-03-30 3:54 AM
I am trying to develop an st-link utility external spi flash loader using STM32F411RE and Winbond W25Q32. Mass erase, Read, Sector erase are working well but the program not working, the following errors are pop-up
1)Timeout during flash programming.
2)Error occurred during program operation!
3)Programming error @: 0x000010AC.
I also attached my full project file, please review and give suggestions
2021-03-31 10:31 AM
Hello @User16438042334827474767 and welcome to the STM32 Community,
Which version are you using ?
Could you try STM32Cubeprogrammer software. Then, please let me know if this solved your issue.
Imen
2021-04-01 1:09 AM
1)I used the version attached, please check
2) I also tried the cube programmer v2.4.0 , but I got the same result but new things happened. First mass erases work well and again when I do the same the mass erase fails. My log is given below.
13:34:36 : Disconnected from device.
13:34:37 : ST-LINK SN : 0670FF535155878281143214
13:34:37 : ST-LINK FW : V2J37M26
13:34:37 : Voltage : 3.25V
13:34:37 : SWD freq : 4000 KHz
13:34:37 : Connect mode: Normal
13:34:37 : Reset mode : Software reset
13:34:37 : Device ID : 0x431
13:34:38 : UPLOADING OPTION BYTES DATA ...
13:34:38 : Bank : 0x00
13:34:38 : Address : 0x40023c14
13:34:38 : Size : 8 Bytes
13:34:38 : UPLOADING ...
13:34:38 : Size : 1024 Bytes
13:34:38 : Address : 0x8000000
13:34:38 : Read progress:
13:34:38 : Data read successfully
13:34:38 : Time elapsed during the read operation is: 00:00:00.008
13:34:49 : MASS ERASE ...
13:34:57 : Mass erase successfully achieved
13:34:57 : UPLOADING ...
13:34:57 : Size : 1024 Bytes
13:34:57 : Address : 0x8000000
13:34:57 : Read progress:
13:34:57 : Data read successfully
13:34:57 : Time elapsed during the read operation is: 00:00:00.007
13:35:10 : MASS ERASE ...
13:35:15 : Error: Mass erase operation failed.Please verify flash protection
13:35:19 : Memory Programming ...
13:35:19 : Opening and parsing file: images.bin
13:35:19 : File : images.bin
13:35:19 : Size : 101252 Bytes
13:35:19 : Address : 0x00000000
13:35:19 : Erasing memory corresponding to segment 0:
13:35:20 : Erasing external memory sectors [0 24]
13:35:25 : Error: failed to erase memory
13:35:25 : Error: failed to erase memory
2021-04-01 1:52 AM
Hi @User16438042334827474767 ,
I recommend you to update the STM32Cubeprogrammer V2.7.0 and upgrade the ST-Link firmware version (go to ST-LINK>firmware update), then try again and tell me if that solve the issue.
I added the right topics to your question in order to increase its chance to be reviewed by our experts.
Hello @Houda GHABRI
Can you please help @User16438042334827474767 on this issue.
Thanks
Imen
2021-04-01 2:43 AM
thanks for your suggestions but still have the error
2021-04-01 2:48 AM
15:16:11 : Disconnected from device.
15:16:12 : ST-LINK SN : 0670FF535155878281143214
15:16:12 : ST-LINK FW : V2J37M26
15:16:12 : Board : NUCLEO-F091RC
15:16:12 : Voltage : 3.24V
15:16:12 : SWD freq : 4000 KHz
15:16:12 : Connect mode: Normal
15:16:12 : Reset mode : Software reset
15:16:12 : Device ID : 0x431
15:16:12 : Revision ID : Rev A
15:16:12 : UPLOADING OPTION BYTES DATA ...
15:16:12 : Bank : 0x00
15:16:12 : Address : 0x40023c14
15:16:12 : Size : 8 Bytes
15:16:12 : UPLOADING ...
15:16:12 : Size : 1024 Bytes
15:16:12 : Address : 0x8000000
15:16:12 : Read progress:
15:16:12 : Data read successfully
15:16:12 : Time elapsed during the read operation is: 00:00:00.007
15:16:31 : MASS ERASE ...
15:16:39 : Mass erase successfully achieved
15:16:39 : UPLOADING ...
15:16:39 : Size : 1024 Bytes
15:16:39 : Address : 0x8000000
15:16:39 : Read progress:
15:16:39 : Data read successfully
15:16:39 : Time elapsed during the read operation is: 00:00:00.007
15:16:51 : Memory Programming ...
15:16:51 : Opening and parsing file: images.bin
15:16:51 : File : images.bin
15:16:51 : Size : 101252 Bytes
15:16:51 : Address : 0x00000000
15:16:51 : Download in Progress:
15:17:56 : Error: failed to download Segment[0]
15:17:56 : Error: failed to download the File
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.