cancel
Showing results for 
Search instead for 
Did you mean: 

Enabled the RTC_CLOCK_SOURCE_LSE in RTC_TimeStamp example application

Nagaraj1
Associate II

Hi,

I am trying to use the RTC_TimeStamp example application provided with the STM32H743I-EVAL board, I've enabled the RTC_CLOCK_SOURCE_LSE in main.h to use the Low-speed external oscillator as a clock source for the RTC.

The problem is that even though i enabled the LSE, when i power cycle the board, RTC doesn't keep up the latest time, it resets to the old time only. When i refer to the user manual of the eval board, to provide OSC32_IN, the R18 to be removed and SB1 shall be closed. Can you please confirm, without making these HW changes, the LSE cannot be configured?

Thanks

Nagaraj

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

You misunderstood: the definition of RTC_CLOCK_SOURCE_LSE means using the 32768Hz crystal X2 on the EVAL board. SB1 (if set) is there to feed OSC32_IN when using an EXTERNAL clock of 32768Hz, i.e. from a clock source existing outside the EVAL board.
So you should leave R18 populated (or restore it with a solder bridge) and leave SB1 open.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.