2023-01-13 1:54 AM
I'm interfacing Nucleo-H753ZI with DAC8775EVM through SPI4.
DAC8775EVM works on logic HI in range of 5V and expects the same logic from Nucleo-H753ZI
but Nucleo-H753ZI MCU itself runs at 3.6V so Logic Hi isn't read by DAC8775EVM.
How to Change the logic level "HI" of SPI4 in Nucleo-H753ZI?
Thanks in Advance.
Regards,
Naveen
2023-01-13 2:21 AM
Hi Naveen,
The level of the SPI signals can be converted between 3.3V and 5V using a level shifter.
Does it answer your question?
Regards
/Peter
2023-01-13 11:15 PM
Hi Peter,
Is it possible to use microcontroller SPI pins to pull up to +5v and use them instead of level shifters. We are preferring this method as the Hardware is designed without Shift registers already.
Regards,
Naveen.
2023-01-14 8:07 AM
Check if the pins in question are FT (5V tolerant) per Data Sheet.
If they are you can use a pull-up and Open-Drain mode for the output.
Check what the reported VIH threshold is for DAC8775 really is, vs level seen on pin/connection.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.