STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST-link v3 mods vs mini connector

The new mods variant comes without a connector. Do the 14 strips on it’s down side correspond to the CN5 STDC14 connector of st-link mini? Cannot find this in the UM2502. Would like to solder wires to these strips rather than to castellated edge. And...

Pavel A. by Super User
  • 5635 Views
  • 6 replies
  • 1 kudos

Connection of MIS2DH

Can anyone give me an explanation about STM 32 micro controller board connection with MIS2DH accelerometer. Can it connect with 2 MIS2DH at the same time? Im really need to know about it cause i need to use two accelerometers at the same time. If it ...

Resolved! Slow code stepping during debug

I'm using a NUCLEO-H563ZI board with the onboard st-link, Cube IDE 1.12, on an intel mac running macos 13.4.1. What I'm observing is that when I start a debug session is that if I set a breakpoint and hit continue i'll hit the breakpoint almost insta...

jperrin by Associate II
  • 2691 Views
  • 2 replies
  • 0 kudos

STLINK-V3MODS programming API and JTAG access.

Hello,I'm using a STLINK-V3MODS in a test and programming interface that I realized for my PCBA. Currently I use the bridge API to manage SPI, I2C, CAN and GPIO interfaces through a software written in Cpp on Qt platform. I would like to perform the ...

ATPG by Associate II
  • 1273 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.