2017-08-08 1:52 AM
Hello,
i want to make my own layout with the STM32F103CBT6 as ST-Link, and im not sure, if i can use this Chip as out of the Box ST-Link or if i have to put some firmware on it to use it this way. My Intention is, to use the ST-Link similar to the NUCLEF303RE-Board (see Attachment page 3 of 4). Thanks!
#firmware? #nucleof303 #st-link #stm32f103cbt62017-08-08 2:44 AM
Hello
steffen.jahnke
,STM32F103 is empty when you buy it. You have to flash program with ST-Link binary file and then you can use it as ST-Link programmer.
Best regards,
Tilen
2017-08-08 2:52 AM
Hello
Majerle.Tilen
,thanks for your answer! Iam new in ST-Programming. Could you tell me where to find that binary file? And which software do i need to flash the binary on the controller? Thanks a lot!
Best Regards,
Steffen
2017-08-08 5:08 AM
Tilen,
did you try? In my understanding, ST-Link is started by a bootloader, and ST does not officially distribute the bootloader image.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.