2019-04-15 8:20 AM
Hello ,
I'm trying to load my project using Atollic TrueStudio V9.2.0 with the ST-Link V2-1 debugger of the nucleo-64. I get this error :
STMicroelectronics ST-LINK GDB server. Version 5.1.0
Copyright (c) 2018, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\Atollic\My_Project\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
Device connect error
Error in initializing ST-LINK device.
Reason: Failed to connect to device. Please check power and cabling to target.
The connection works with the ST-LINK utility, but it's still not working with Atollic.
I updated the last version of ST-link USB driver and I did upgrade the ST-link firmware (V2J31M21).
I thought the problem with the initialization because in the config.txt file of GDB server i had :
persistant mode enabled (-e)
verbose mode disabled (# -v )
SWD mode enabled (-d)
which is not the case in the Atollic console but i tried to uncomment the verbose mode line but the permission is denied.
Any ideas how to solve this problem ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.