2023-12-12 10:13 PM
I was looking at the schematic of a ST STM32H743I-EVAL board and noticed it uses a voltage level translator to connect a SD CARD to STM32H743 and used a separate LDO to produce 2.9V for the SD side.
The custom hardware I'm designing has a 176 pin STM32H743II supplied with 3.3V only. Now I couldn't find more information on this but is it really necessary to use a voltage translator at all?
I would rather not use a translator with that BGA package or any other unnecessary IC for that matter.
Solved! Go to Solution.
2023-12-13 1:58 AM
Hello,
we have the STM32H747 discovery board that features an sdcard interface with only an ESD protection, and no level shifter,
please have a look:
Shouldn't be different for the STM32H743.
In any case, please check the SDcard specifications for what is needed depending of what kind of card you want to support:
2023-12-13 12:49 AM
when inserts SD card, there is a voltage drop for 3.3V rail. it should be better to add a dedicated LDO for SD card.
2023-12-13 1:33 AM
Thanks. That actually makes sense. Plus I'm gonna need an ESD protection so I figured it is better to use voltage level translator with ESD protection and a QFN package like TXS02612 and a LDO.
2023-12-13 1:58 AM
Hello,
we have the STM32H747 discovery board that features an sdcard interface with only an ESD protection, and no level shifter,
please have a look:
Shouldn't be different for the STM32H743.
In any case, please check the SDcard specifications for what is needed depending of what kind of card you want to support:
2023-12-13 6:13 PM
STM32H743I-EVAL supports SDIO3.0 interface microSD™ card while STM32H747I-DISCO supports SDIO2.0 interfacemicroSD™ card. They are different SDcard specifications.
2023-12-13 6:48 PM
You don't need the transceiver. Only used for high speed ultra modes. Should be able to clock 50+ MHz at usual voltages without them.
https://community.st.com/t5/stm32-mcus-products/stm32h753vit6-sd-card-sdr104/m-p/614777
2023-12-13 11:21 PM
Interesting. Does it have anything to do with the voltage translator?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.