STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Connecting G0 Nucleo board to Linux

I've been running into issues with my G0 Nucleo board in that I can't seem to get it to connect properly to my Linux machine via STLink. I've gone through and added the requisite rules, but even so if I list USB devices, the board is conspicuously ab...

JAppe.1 by Associate II
  • 3919 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F401re external power

Hello everyone.I'm trying to run my project with external power supply (5V on Vin or E5V) but the problem is that I always have to press the reset button to start the code normally when I connect it, if the board is powered by the USB port the progra...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.