2023-03-28 6:25 AM
I have a custom board on which there is an STM32 microcontroller. The board doesn't include the ST-LINK so I bought it and connected it to the board for the debug. After that my pc cannot detect the COM port anymore. Somebody can help me? Thanks
2023-03-28 6:28 AM
The stand alone ST-LINK/V2 doesn't have a UART, that is a V2-1 feature.
Get an ST-LINK/V3SET or use a serial dongle.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.