2022-10-03 7:39 AM
In STLink upgrade download for linux, in the following path:
stsw-link007/readme.txt
titled STLink firmware upgrade applications
the following text paragraph:
"On Linux, users must be granted with rights for accessing the ST-Link USB devices. To do
that, it might be necessary to add rules into /etc/udev/rules.d. This can be achieved by
running one of the package provided into the subdirectory StlinkRulesFilesForLinux."
A jargon action of running a package which has no choice criteria into a non-existant subdirectory needs clarification as to what specific actions are needed.
Hal
2022-10-06 12:20 PM
The fix appears to be:
"This can be achieved by running one of the packages provided in the subdirectory StlinkRulesFilesForLinux using , e.g., the following command:
"sudo cp 49-stlink-v3.rules /etc/udev/rules.d"
ST comment?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.