2020-01-22 6:44 PM
Hello! I have problem with booting NUCLEO-G431RB board.
There was no problem before I changed some registers.
I changed option bytes as below and now I cannot boot the board.
(in the user code part at main)
(I tried to change nSWBOOT bit as below)
/////////////
HAL_FLASH_Unlock();
HAL_FLASH_OB_Unlock();
FLASH_OB_UserConfig(OB_USER_nSWBOOT0, 1);
HAL_FLASH_OB_Launch();
////////////////
build was completed but there was problem when I tried debug with that code
(I bebug with ST-Link(ST-LINK GDB server))
At the First time, I can enter to debug session and there was problem at line HAL_FLASH_OB_Launch();
But this is not my question
After several times of debug again, I can't even go to debug session because of error.
(I didn't change the code)
The error message is
//////////
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load (my elf file location)
///////////////
Let me show you my console message
//////////////////////
STMicroelectronics ST-LINK GDB server. Version 5.4.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.3.0
-------------------------------------------------------------------
ST-LINK SN : 002500463137511233333639
ST-LINK FW : V3J4M2
Voltage : 3.29V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x468
Device name : STM32G43x/G44x
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M4
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a41664.srec
File : ST-LINK_GDB_server_a41664.srec
Size : 16076 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 7]
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.2.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.1.0.201910081157\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
///////////////////////////
I searched How to solve this problem but I can't find solution.
I'm waiting for you help!
Any comments will be very helpful.
////////////////////
And for you information, Let me tell you error at stm32CubeProgrammer.
I notice the program after all the above things, and I connect the board with the program and there is error as below
Error: Data read failed
Memory & File edition tab doesn't works, but i can apply and read Option bytes at Option bytes tab
I hope you can get hint from here!
Thankyou
2020-01-24 3:24 AM
You mention that you can apply and read option bytes but... can you erase the chip with CubeProgrammer stand-alone? And if so, are you able to get the board functioning again with another project? To just blink a LED or something to make sure the code is on the target.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.