Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi,I'm going to say that this is a really nooby question, however I cannot find the answer anywhere.Background, I'm using a nucleo F103RB, and I've programmed it using CubeIDE. I can connect the board, debug and run the program fine. The board is po...
Hello I just bought the STM32L152C-DISCO board. The board worked with its original firmware, but I can't use it with CubeIDE to create my own programs. I create empty STM32project using Board Selector option: I made a simple program to make the LEDs...
HI,I am facing an issue where my ST-Link V2 is not detected in STM32CubeIDE while trying to connect to my STM32F303RCT7 board. Below are the details::small_blue_diamond:**Issue Description:** - ST-Link V2 is connected via USB, but it is not detected ...
When I try to debug from CubeIDE, I get this error.But I can connect with STLink-Util and flash a firmware just fine.What does this claim there was "no device" on target, mean exactly?The firmware has worked previously, but there is a bug now in my f...
Hi all, I have no experience in designing a schematic, and I want to design one for my project where I will be using an STM32C0 with an RFM95. I also want to include a LiPo charging circuit, but I’m not sure if my design is correct, especially the Li...
Good afternoon, I am currently trying to calibrate my ADC4 of my NUCLEO U545 and I am using the following function: HAL_ADCEx_Calibration_Start(&hadc4, CalibrationMode, SingleDiff);As said before the first parameter is going to be the ADC4 that I am...
Hi evryone,I'm trying to start a project with Trustzone activated, so I followed that tutorial by ST and I'm using exactly the same board the STM32L562E-DK but when I'm trying to flash the programm on the board I got that error:And there is the log f...
Initially, I ran a program from Simulink onto my STM32H755ZI, but I encountered an issue where only one core was functional, even though the STM32H755ZI has two cores. This led to the error "No device found on target."As I continued troubleshooting a...
Hi,I am experiencing an issue with my ST-Link V2 debugger. When I connect it to my PC, I often receive the error: "USB device not recognized: Unknown USB device (Device Descriptor Request Failed)" and ST-LINK orange LED turns on. However, after sever...
Hello everyone,During some test I try to change the type of the StLink-V3 of the NUCLEO-H7A3ZI board to "STM32 Debug + VCP"After this I can't flash or connect to the board even if I update back to "STM32 Debug + MAss storage + VCP".I try to erease th...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.