Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello, I have seen in the post That many users had a problem with the LDO power supply for STM32H757ZII wanted to ask, can you confirm that I have a correct implementation of the power supply for LDO?
hi im using stm32g474vet6 mcu , im using spi in dma mode of both tx and rx and made dma in circular mode.what happens means when i start a first tx or rx itself spi clk is coming continuously. what to do , it is due to circular mode.if (send_spi_cmd ...
I m trying to communicate through USART with my NUCLEO-L476RG but the STM console is displaying nothing. I have created a simple project:I m overriding the __io_putchar function:int __io_putchar(int ch) { if (ch == '\n') { uint8_t ch2 = '...
I am making a stm32f411ce board and I want make sure everything works because it's very expensive to order a pcb in my country. I want to use components like Hc-49 8mhz crystal(and dt-38 32.768khz) oscillators with ceramic PTH capacitors, the only sm...
HI there, I own a couple of STM32H747-DISC0 boards for a year. I been using them without issues debugging but when started a new project, I do not know what went wrong that cannot access to any core from any ST tool (CubeIDE or CubeProgrammer).No mat...
I bought a 1Set STM32F407VET6 Industrial Control Board from AliExpress to evaluate the STM32 MCU family but I can't find any information about it. 1Set STM32F407VET6 Industrial Control Board I've used many different Arduino, Teensy, ESP32 and other s...
[translated] When using STM32H755ZIQ-NUCLEO, the firmware upgrade fails due to data cable, and there is no way to download the program, is there a solution for you?
I have a Nucleo WB55RG board with in built ST-Link.I programmed it with a blinky LED & a UART message "Hi there!\n" via the CubeIDE on a different PC & it all works fine. TeraTerm has no problem selecting the ST-Link device connected to the PCNow run...
Hi,I am currently working with the STM32C091CBT6 microcontroller and am looking for suitable development hardware.My primary questions are:Is there an official STM32 Discovery kit or Nucleo board specifically designed for the STM32C091CBT6 microcontr...
Hi,I want to generate a timeslot control signal consisting of one 10-microsecond pulse followed by fifteen 2-microsecond pulses.I want the period to remain constant, aligned on the falling edge.My problem is that before and after the long pulse, the ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.