STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo STM32F411RE

After I load my code ( with help of IDE) into NUCLEO MCU via USB cable, I'd like to disconnect it (disconnect USB cable) and power NUCLEO with battery(s) or external power supply ( lets say 3V or 5V). Is there any PDF where to read ? Or brief explana...

Roman_E by Associate III
  • 723 Views
  • 1 replies
  • 0 kudos

Resolved! Nucleo-G491RE and opamp1

I am using Nucleo-G491RE. I am debugging through the built-in ST-Link using STM32CubeIDE 1.18.1. My design uses opamp1 in standalone mode, which assigns OPAMP1_VOUT to PA2 and OPAMP1_VINM to PA3. What configuration of solder bridges will bring these ...

Connecting B-CAMS-IMX with Stm32n657x0-Q

Hello,We would like to know if it is possible to connect the STM32N657X0-Q board with a B-CAMS-IMX camera. If so, what would be the best way to verify that the connection is successful and that the camera is working properly?Any guidance or documenta...

Dila by Associate
  • 1643 Views
  • 3 replies
  • 0 kudos

Resolved! STM32N6 Boot Pins

Hello, I have the STM32N6570-DK kit. I can compile, upload and debug by following the instructions on the kit. I designed my own board but I can't debug. I'm reviewing all the possibilities and I noticed some problems. I couldn't find any explanation...

Okeskin_0-1750684981208.png Okeskin_1-1750684998046.png Okeskin_2-1750685049416.png Okeskin_3-1750685155649.png
Okeskin by Associate III
  • 2631 Views
  • 6 replies
  • 2 kudos

Resolved! I2C between two NUCLEO-F446RE boards

Hi, I am trying to use a Nucleo-F446re as master and another one as slave. But the master is probably being timed out (not sure). Can you guys please have a look at my code and configuration. Thanks in advance <3  My Wiring:1. I connected PB8 & PB9 o...

Asif17r by Associate II
  • 3777 Views
  • 9 replies
  • 5 kudos

Resolved! Looking for NUCLEO-L496ZG schematic

Bonjour ! Je travaille avec une carte NUCLEO L496ZG. Maintenant, j'aimerai intégré le STM32L496ZGT6U dans mon projet mais j'ai besoin du schéma de la carte NUCLEO pour étudier certains points. Où puis-je trouver ce schéma ?Merci d'avance !Google tran...

antho21 by Associate
  • 1296 Views
  • 2 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.