2017-08-19 11:48 AM
An ST-Link (from Nucleo-64) don't want to read an STM32F030RCT6 under Windows 10 (64 bit) with a message 'Can not connect to the target'. The most interesting thing is it reads an another same board already programmed. But this doesn't mean the clear board is broken: it could be read with the same programmer but another computer with Windows 7 (32 bit). With that computer, both boards communicate with the ST-Link. STM32 ST-Link Utility, STLinkUSBDriver, and ST-Link_CLI versions are same on both computers. So I couldn't understand what to do and what I have to change?
#st-link #windows102017-08-19 1:44 PM
They have the same ST-LINK firmware? Try updating that to current.
Check also 'Connect under reset' settings, or perhaps pull the BOOT0 pin high on the problem device.
2017-08-19 4:01 PM
I used one ST-Link and board on both computers. And, of course, I've updated everything I could update. I've tried to connect under reset and all other possible modes. And only after that, I wrote the previous message. At Monday I'm going to check every signal with an oscilloscope.
2017-08-21 8:54 AM
I've checked signals with an oscilloscope. It seems a port responsible for NRST signal is burned out. Sometimes access to an MCU is successful, sometimes not, but a shape of the NRST is far from normal.
By the way, how to say in English that a chip is broken but not fully like in this case?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.