STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

reprogramming Nucleo-F767ZI

Hello all,i work at the moment wit Nucleo-F767ZI. The ST-Link Board is already separated but i must reflash the µC again. I've already seen in STM32 Nucleo-144 boards User manual, which pin i need. Is there a connector on nucleo board itself, that i ...

Zefry by Associate
  • 753 Views
  • 0 replies
  • 0 kudos

Resolved! Minimal configuration of STM32F410RB to enable recognition/programming by ST-LINK/V2-1

I've used a Nucleo-F410RB to develop my application. I'm now trying to minimally configure the chip (STM32F410RB) on a separate PCB breakout board (LQFP64 package) after studying the schematic diagram and specs in the Nucleo documentation. Sadly, I c...

0690X000006C7KKQA0.png
DGold.11 by Associate II
  • 2023 Views
  • 3 replies
  • 0 kudos

Read from chip and program

Hi,My application requires configuration based on certain input received via uart. This input will be stored in flash memory of the chip and the application runs with those configuration. Now, I need to program a certain of such device with the same ...

ST-link utility V4.2 on STM32L4S5

Hi, I've had some issues while protecting some flash memory pages on STM32L4S5 using ST-LINK V4.2. In fact, When i choose the page 256, The ST-LINK performs the protection on the page 0.To verify this issue, please clic agin on option byte after app...

MELMA by Associate
  • 1186 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.