STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to get started programming STM32

I'm attempting to program a blue pill stm32 but I'm plagued with software issues/errors and im in need of some advice/help. The issue is with the st-link v2 working in tandem with keil. It only works for the first time a try to flash the board and no...

HNann by Associate
  • 1506 Views
  • 2 replies
  • 0 kudos

What load capacitance should be soldered for an 8MHz crystal for an STM32F446RE Nucleo board?

Hi, guys. I boughtSTM32F446RE, mbed-Enabled Development Nucleo STM32F4 MCU 32-Bit ARM® Cortex®-M4 Embedded Evaluation Boardhttps://www.digikey.com/product-detail/en/stmicroelectronics/NUCLEO-F446RE/497-15882-ND/53477128MHz ±10ppm Crystal 18pF 80 Ohms...

0690X000006DMA5QAO.png
Matthew K by Associate II
  • 1155 Views
  • 0 replies
  • 0 kudos

Resolved! Given the correct hardware configuration, is it possible to access two different external memory types (SRAM and Flash) by use of the same FSMC bus?

I have an application where it is necessary to read data from external flash to perform operations on data stored in external SRAM by using the same fmc connections. In this case the parallel interface is important as the operations are time sensitiv...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.