2019-02-05 7:03 PM
I'm attempting to program a blue pill stm32 but I'm plagued with software issues/errors and im in need of some advice/help. The issue is with the st-link v2 working in tandem with keil. It only works for the first time a try to flash the board and not any other attemps to flash the board.
other info:
I used STM32CubeMX to generate the code based on my specific MCU(STM32F103C8...) and built it in keil.
2019-02-06 1:44 AM
Hello,
Try to upgrade the ST-Link firmware version to V2-1 through the STSW-LINK009, then disconnect and connect your board.
Otherwise, you can use the STM32CubeProgrammer software for programming STM32 products.
Kind Regards,
Imen
2019-02-06 2:21 AM
> It only works for the first time a try to flash the board and not any other attemps to flash the board.
Check that your example code does not use the JTAG pins as GPIOs, and that it does not employ any sleep mode.
Those use cases could make debugger access a bit finicky.
As last resort, you can use the Flash Loader Demonstrator software, and do a Flash mass erase after booting into system mode.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.