STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Nucleo-64 for STM32L073 gets very warm

I got a STM32 Nucleo-64 for STM32L073 board from Farnell. A few seconds after I had connected it to my PC via USB, it got so warm that I could not touch the CPU. They then send me another one, but it has exactly the same problem. I have tried setting...

KKark by Associate II
  • 2045 Views
  • 2 replies
  • 0 kudos

[Very Urgent Help] The STM32F042K4T6 integrated sometimes does not work. I'm restarting the system from the NRST pin. If I'm throwing resat 10 times, the system works in 8 and the microcontroller does not start in 2 of them.

Hello EveryoneI design oven timer (transformerless) with STM32F042K4T6. Although I tested everything separately there is a problem in the pcb. When the system first comes on, the system works but sometimes it doesn't. I tested it 10 times and the MC...

0690X000009YwaaQAC.png 0690X000009YwcCQAS.png 0690X000009YwcgQAC.png

ST-LINK for USB UART stops working

We use STM32H7 NUCLEO board. The connection is done via UART to the host via the UART ST-LINK interface (using the USB VCP bridged by the 'Debug MCU' and the main CPU).On some boards, it works fine, forever. On some other board the connection gets lo...

STM32 Discovery kit for STM32L475 MCU

I have a STM32L475 and when i connect my mcu to my computer , i can not get any signs from pc that i connect a usb driver to my Pc and when i went into the device manager and checked the disk drivers there is no st-link Usb connected.I installed the ...

BBenc by Associate
  • 785 Views
  • 0 replies
  • 0 kudos

When using an stlink V2-1 in external mode, can MBED drag-and-drop programming be used?

Several Nucleo boards come with an embedded stlink V2-1 which supports MBED programming by copying the firmware binary to a USB mass storage device. If the programmer is snapped off the board and put in to external mode, does this method of programmi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.