2019-07-15 12:49 AM
The manual states two MX25QL512ABB8ESF-0SIT from
Macronix are fitted. That's wrong, there is no such device made by Macronix, in fact there are two MT25QL512ABB from Micron on the board (in accordance with the schematics).
2019-07-18 4:45 AM
Hi @Andreas Bolsch ,
You are right, this is an error on UM2411 and it is reported internally to be fixed.
As you said, the correct one is MT25QL512ABB8ESF-0SIT (FBGA code = RW187) from Micron.
Thanks for bringing this error to our attention.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.