Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I have connected STM32F413vht6 JTAG pins TMS,TCK,TDI,TDO,TRST,VCC,GND to ST-LinkV2 programmer. We get the error message "No target connected".tried connecting NRST connected to GND with "connect under reset" option. still the same issue. Please sugge...
Hello there,I was looking for the information about the part number of the STDC14 connector in the STLINK-V3SET device as I want to replicate it on a shield, but could not find any. Would appreciate all help.Also, I have just noticed that the dimensi...
Hi there, we are getting started with a NUCLEO-L412RB-P evaluation board, which has a stm32L412RBT6PU processor on it.According to Section 9.7.1 of the user's guide (UM2206), the default clock is the LSE oscillator, which is "OSC 32khz clock supply."...
Hi ,I am using STM32H745 Discovery board and trying to connect to target ,but it is giving an error prompt of cannot connect to target. Actually I have made changes in the option bytes that is by mistake I have unchecked both the BOOT_CM7 and BOOT...
Hi! I wanted to start with P-L496G-CELL02. I followed all instructoins from website (video), I have Drivers etc. installed, but in Tera Term I have not got any welcome messages, even my Voucher Cod, so I can't add a new board on https://stm32-c2c.com...
Hi,I have a NUCLEO-L412KB board, debugging with Segger embedded studio. Since it is not possible to connect the Segger debugger box to the board (SWD is not connected to connectors) I used the on board ST-Link as J-Link (converted with programme STLi...
Hello,there's a problem with this version of stlink server on new MacOS Catalina. When I upgraded my system to new OS version, everything was working fine, but after clean reinstall I was not able to install this software.I think the installer is blo...
When i try one controller(stm32f103c8t6) its show details like this .When i connect other controller(stm32f103c8t6) its show the error like this. Please some one help to resolve this error.
HelloHow it is possible to perform a pin reset with the STLINK/V2 using STM32CubeIDE and GDB after programming?Debug probe: ST-LINK (ST-LINK GDB server)Interface: JTAGReset behaviour Type - no HARD/PIN reset available !?
Such an equipment is literally nowhere to be find, could You help me find required adapter and cable? I'm sending photos, hope it helps.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.