STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to test if a MCU is broken?

Hi all!I have developed a PCB with a stm32f4 MCU. The MCU can be programmed through SWD and works well. However, the current consumption of the whole PCB is high (~190 mA at 3.3 V). When I erase the chip, the current consumption becomes 120 mA. Could...

MCUser1 by Associate
  • 2890 Views
  • 3 replies
  • 0 kudos

why can't i update my st

I am trying to connect my stm32f103C8 via usb, when I did this I got the following message "Error in initializing ST-LINK device.Reason: (4) No device found on target".I try to update it with the stm32utility and it doesn't recognize the card.How can...

DQuir.1 by Associate II
  • 1166 Views
  • 1 replies
  • 1 kudos

About STM32G0 series and BOOT0 Pin

Hi, i have a question about this. Normally we use F0 series and BOOT0 pin must be connected to GND via 10K Ohm. So, BOOT0 pin were apart. But now, BOOT0 pin and SWCLK pin is same. I created a new schematic and I connected BOOT0/SWCLK to GND via 10K ...

Resolved! Nucleo H743ZI2 - PC8 not connected to CN12? The User Manual for the Nucleo H7 devices says that PC8 is connected to Connector 8 Pin 2 and Connector 12 Pin 2 (pages 39 and 42). However on my boards it doesn't seem to be connected to Connector 12 Pin 2.

Unfortunately I have already designed my PCB and am now hoping that I just forgot to set a jumper or whatever, but I could not find anything about it in the User Manual. Maybe someone can measure on his or her board to see whether I am mistaken.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.