2020-03-13 6:14 PM
I am trying to connect my stm32f103C8 via usb, when I did this I got the following message "Error in initializing ST-LINK device.
Reason: (4) No device found on target".
I try to update it with the stm32utility and it doesn't recognize the card.
How can i fix this?
2020-03-14 2:49 AM
Make the target functional and connect it properly?
For an external ST-LINK/V2 make sure pin 1 is connected to the board supply and the voltage is correctly reported in the debug logs of the ST-LINK Utilities.
Check SWDIO and SWCLK pins.
Check supply pins on chip
Check NRST level
Check chip orientation
Perhaps explain your system with more detail?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.