Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I am looking for reference design for STM32L051K8T6TR to quick start schematic and layout for basic controller interface.
Hello!I'm trying to program multiple STM32F432VIT6 MCUs at the same time, from the same computer using many ST-LINKV2 connected via USB.I want it to be automatic so I'm using the ST-LINK Utility CLI to program them via C#.So far I've been able to lis...
Hi,My St-link on board the STM32F7508-DK is corrupted and i cannot flash it over usb anymore.I've manage to find a Stlink V2 binary and it works ok for flashing but not for debugging.Also the V2 version does not have the ST-link in mass storage for d...
Why do I get this error when I try to connect STM32CubeProgrammer via ST-LINK to STEVAL-PTOOL2V115:22:48 : STM32CubeProgrammer API v2.5.015:22:50 : ST-LINK SN : 56FF6606518252503838128715:22:50 : ST-LINK FW : V2J37S715:22:50 : Board : --15:22:50 : V...
I am struggling with debugging of STM32f407VGT6 mcu. I use discovery board as ST-LINK for debugging. Done below instructions:- All connections between st-link and uC- Power distribution controls (VCC, GND)- CN3 jumpers not connectSh...
Hello,I am searching for the input/output impedances for my STM32L476RG microcontroller and I can't find any information in the microcontroller datasheet or else where on the web. Are those values given in any documentation? If not, can they be calcu...
ST marked several Disco boards as NRND (i.e. discontinues them).Some of them are easily replaceable - e.g. the 'F0308 by the 'F0, the 'L100 by the 'L152, the 'F7308 (which btw. is only a few months old) by the probably completely identical (except fo...
I'm trying to flash/debug a B-L072Z-LRWAN Discovery kit from Ubuntu 20.04 using openocd, but its failing to connect:openocd -f interface/stlink-v2-1.cfg -f target/stm32l0.cfgInfo : auto-selecting first available session transport "hla_swd". To overri...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.