2021-01-18 3:32 AM
Hello!
I'm trying to program multiple STM32F432VIT6 MCUs at the same time, from the same computer using many ST-LINKV2 connected via USB.
I want it to be automatic so I'm using the ST-LINK Utility CLI to program them via C#.
So far I've been able to list all the ST-LINK devices connected to the computer and to program the board when only one device is connected, but when I connect two devices I can not give the program instruction -P the serial number of the device I want to target.
I think it should be possible since the ST-LINK Utility Tool has a list in which one can select the target device.
I'm following the ST-LINK Utility Manual
Does someone has an idea of how can I achieve this?
Thank you!
Solved! Go to Solution.
2021-01-18 12:59 PM
-c is not one command, it's a switch. You can and shall use several switches simultaneously. The -c switch tells the program, which STLink are you going to use, the -P switch tells, which file is to be programmed.
JW
2021-01-18 4:57 AM
> -P the serial number of the device I want to target.
Where do you get this from?
-P is used to determine the file to be programmed.
You want to use -c ID=*** or -c SN=xxxx
Syntax: -c [ID=/SN=] [JTAG/SWD] [FREQ=] [UR/HOTPLUG] [LPM]
[ID=]: ID of ST-LINK[0..9] to be used when multiple probes are connected to the host
[SN=]: Serial Number of the chosen ST-LINK probe.
JW
2021-01-18 5:12 AM
The Cube Programmer app might have additional options, but I'm sure it could accept and index.
To scale you might want to use the DLL interface.
2021-01-18 5:14 AM
Hello, thank you for you answer
Maybe I'm not fully understanding the use of the command -c, but how do I load a hex file into a micro using this command? I can specify the SN, but can I flash the device?
2021-01-18 12:59 PM
-c is not one command, it's a switch. You can and shall use several switches simultaneously. The -c switch tells the program, which STLink are you going to use, the -P switch tells, which file is to be programmed.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.