2021-08-27 5:14 PM
Hi! I have this problem with my STM32F401RE and STM32G431RB when i connect the target and try to flash my code with CubeIde, I tried to solve this using ST Link Utility, CubeProgrammer, upgrating drivers but nothings works, my G431 firmware isn't recognized by any program and can't upgrated that, F401 is recognized but doesn't work and had same error (st link and no target found), the F401 and G31 chip are getting hot when are connected, if someone can help to resolve this problem, i will appreciate it.
2021-08-27 5:39 PM
> the F401 and G31 chip are getting hot when are connected
You have a hardware or wiring problem. If it's happening on multiple boards, sounds like the programmer is the problem. Software isn't going to cause that.
What is your programmer and how are you connecting it? Be specific.
Unless these are just nucleo boards, then it sounds like they're damaged or miswired.
2021-08-28 9:07 AM
Hi there! thanks for answering.
•I don't have any pin in use, i just connect the board through the cable to the computer and the chip begins to heat, i use the stmcubeide (with the g431 this problem happened for the first time when the software asked me to update the target to flash)
2021-08-28 11:39 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.