STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Fail to launch openocd GDB server:timeout

Can anyone help me to handle with a openocd issue? I got a message as follow "Failt to launch OpenOCD GDB server:timeout" in VSC. The output message are Info : Unable to match requested speed 1000 kHz, using 950 kHz Info : Unable to match requested s...

clee.10 by Associate III
  • 1224 Views
  • 0 replies
  • 0 kudos

If I remove the SMT32L476RGT6U IC from the Nucleo board first. Then Is it possible to connect SMT32L476RGT6U IC in an external board with STLink pins (CN4) of the Nucleo-L476 (IC is removed) board?

If I remove the  SMT32L476RGT6U IC on the Nucleo L476 board.I will mount the  SMT32L476RGT6U IC on an external PCB.Now, I will connect the required pins of IC with CN4 of the Nucleo Board.Is it possible for debugging for external application? My inte...

0693W00000FApDzQAL.jpg 0693W00000FApEEQA1.jpg

Resolved! With ST-link V3, is there an option to verify while programming like in ST-link V2?

MCU is STM32L0.The file I use to program has option bytes added with read-protection turned ON. :020000041FF8E3 :0C0000000000FFFF7A80857FFF0000FFFA :00000001FFUsing ST-link V3, I'm having this error: (see attached screenshot)  Command line:stm32_prog...

0693W00000FAUPBQA5.png
FArdi.1 by Associate III
  • 4167 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.