2021-09-10 9:28 AM
As above, have a project I'm porting from one custom board to another. Using the same external crystal (8Mhz) and virtually identical circuitry with the exception of a few custom ASICs. This code works fine on the L432, but when I run it on the L496 (debugging via STLink pod) I get a timeout while waiting for HSE to go ready.
/* Enable HSE BYPASS to PLL */
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
/* Initialization Error */
ClockError();
}This is directly from the ST LIbrary file stm32l4xx_hal_rcc.c; I hit this timeout every time waiting on HSE. Brought the timeout value from 100mS default to 500mS, no change.
/* Set the new HSE configuration ---------------------------------------*/
__HAL_RCC_HSE_CONFIG(RCC_OscInitStruct->HSEState);
/* Check the HSE State */
if(RCC_OscInitStruct->HSEState != RCC_HSE_OFF)
{
/* Get Start Tick*/
tickstart = HAL_GetTick();
/* Wait till HSE is ready */
while(READ_BIT(RCC->CR, RCC_CR_HSERDY) == RESET)
{
if((HAL_GetTick() - tickstart) > HSE_TIMEOUT_VALUE)
{
return HAL_TIMEOUT; //Times out at 200mS (default was 100mS)
}
}
}
2021-09-10 12:13 PM
Are these custom boards? Are you feeding in an HSE clock source?
2021-09-10 1:47 PM
Sorry, I had given some more detail in an earlier edit of the post then realized I wasn't describing the issue correctly.
Yes, they are custom boards. This exact custom board previously worked with a STM32F205; I had it reworked with a STM32L496 (same package) and now am trying to port some (also previously working) FW from a very slightly different custom board that was running an STM32L432. I know that's a bit confusing; chip shortages have a lot of people scrambling.
I have an 8MHz crystal feeding HSE; I verified the crystal is oscillating.
2021-09-10 1:52 PM
2021-09-13 11:00 AM
Correct. I am switching to PLL as the HSE source.
/* Enable HSE BYPASS to PLL */
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
/* Initialization Error */
ClockError();
}The issue is that HSE never goes ready, so this times out:
/* Wait till HSE is ready */
while(READ_BIT(RCC->CR, RCC_CR_HSERDY) == RESET)
{
if((HAL_GetTick() - tickstart) > HSE_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
2021-09-25 2:30 PM
You were told that HSE bypass mode is not for crystals, but you are still using it!
2021-09-29 6:36 AM
No. Please re-read my post. I TEMPORARILY switch to the PLL feeding the HSE. It is during this TEMPORARY change that I use bypass mode. And, as I stated, HSE never goes ready.
2021-09-29 7:14 AM
> I TEMPORARILY switch to the PLL feeding the HSE. It is during this TEMPORARY change that I use bypass mode.
This makes no sense. HSE feeds the PLL, not the opposite.
> No. Please re-read my post.
For reference, here's what you said:
> I have an 8MHz crystal feeding HSE; I verified the crystal is oscillating.
So you have a crystal, but it's somehow temporarily not hooked up? And what's hooked up there instead? I've reread your post. It doesn't make a lot of sense. I suspect there is a fundamental misunderstanding.
2021-09-29 9:15 AM
I did understood from the first time that you do not understand how HSE and PLL works. Now go and read the respective sections from the reference manual. ;)
HSE has two modes - the one for crystals and the other one (bypass) for external clock signals. And PLL has nothing to do with it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.