Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi All,I use the STM32H743ZI2-NUCLEO board with JP5 on 1.8V for MCU_VDD.Running the LWIP example, the Ethernet doesn't work (It does work when running with 3.3V).Any idea how to make it work with 1.8V?Thanks,David
Hello. We are working on a project that uses STM32H747 dual-core MCU.The ST-Link firmware is updated to the latest version, so debugging is not working well.So I'm going to lower it to the version I used before, but I can't download it. The lowest av...
Hi, I am looking for STM32F446RE Schematic Diagram. Can any Help me, where to find the Schematic Diagram of STM32F446RE, I have checked the documents of ST(https://www.st.com/en/microcontrollers-microprocessors/stm32f446re.html#documentation) I did n...
When we enable the RTC feature on our controllers, we do a calibration in Production against a GPS-locked 10MHz signal. Usually, we'll use the T2 ETR to clock the 10MHz signal in and an RTC-generated 1Hz signal on one of the other T2 channels such a...
I have 5 versions of the STLINK. For the three newer versions, the VCP on STLINK-V3MODS and STLINK-V3MINI work as expected. I've been using the V3MODS and V3MINI daily for over a year. The STLINK-V3MINIE shows up as a COM port in Windows Device manag...
stm32f412 discovery data MB1209 Board design project filesAn error occurs when you unzip and open the Altium project pcb file.Is it a version issue?stm32f429 discovery Altium project pcb file is OK
I have my own F411 PCB board, on which there are a few devices that MCU/F411 uses I2C1 (I2C HAL) to communicate.Sometimes I2C HAL API (HAL_I2C_Mem_Read, HAL_I2C_Master_Transmit, HAL_I2C_Master_Receive) calls may return with error: most of the time er...
Dear, I have a STM32F446 connect trough QSPI the S25FL064L .I ask if there is the possibility using STLINK and STM32CubeProgrammer to program the S25FL064L .Tell me if there are other solutions to program the external memory trought the STM32F446 by ...
Hi, I'm making a board on which I want to use the STDC14 connector of the STlink V3 programmer for the SWO interface of my MCU.But I have some questions about the pinout, in the manual I find this table:1 - PIN 3 (T_VCC): this pin must be connected t...
I'm waiting for a STM32L4 LQFP48 micro that also includes a DFSDM to become available, it's not urgent and I've got plenty of other things to do. But I have noticed there are a lot of QFN48 parts available. Maybe ST could make an adapter as described...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.