2023-01-03 9:23 AM
Hi All,
I use the STM32H743ZI2-NUCLEO board with JP5 on 1.8V for MCU_VDD.
Running the LWIP example, the Ethernet doesn't work (It does work when running with 3.3V).
Any idea how to make it work with 1.8V?
Thanks,
David
2023-01-12 3:33 AM
Hello @Community member,
Please make sure that R4, R43, R44, R45, R46, R47, R48, R49, R50, R51, R52, R53, R59, R61, U1, U10, U15, and SB45 are not removed.
Because after removing these components, it becomes impossible to use Ethernet with1.8 V.
For more explanation, I advise you to refer at the UM2407.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-12 4:41 AM
Hi Kaouthar,
Thanks for your reply.
The board is at its manufacturing state, no component was removed.
I just moved JP5 to 1.8V and the ETHERNET stopped working.
Any idea why?
Thanks,
David
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.