Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello, i want to measure the power consumption of STM32F767zi only MCU Part using X-NUCLEO-LPM01A. The step of manual says to "open the SB110" by default SB110 is ON what are the ways to make it open ? can we do it through wires or some jumpers?
When connecting a brand new STM32F3348-DISCO board to USB on my MacBook Pro (M1, Ventura), USB communication fails and the ST-Link is not recognised. LD2 flashes brightly red and LD1 flashes hardly visible.Sometimes the communication works for a very...
Hi guysI am using the STM32 Nucleo-144 evaluation board and trying to upload the program by the STM32 ST-LINK Utility.When I try to connect to the board, the console always shows the following error message: "No target connected," "Can not connect to...
At first, I'm an absolute beginner, I'm still on my way to learn more about STM family regarding electronics.Lately I've been having circuit issues with PL2303. After reading datasheet, number 6.2,5V can also be used as input power suppliesI've conne...
Using the STM32L412 I use the PB4 for the signal NJTRST of debug connector and the ST-LINK does not work fine (but it works using J-LINK). We use also H723, H743, L476 and L496 connecting NRST to debug connector. This can be done with L412?Best Reg...
Currently I am using STM32 Nucleo-L152RE , so i want eagle schematic file for that also to take reference for my pcb hope you will help me
Hi, I have some questions about the connection and its external components for the SMPS step-down converter of the MCU.The microcontroller I'm using is a STM32H745IIT6. On the datasheet I found this schematic and these indications for the components:...
I cannot find the logic in the schematics about the mapping of the 2 stmod+ connectors.Which pins of the stmod+ correspond to the MCU pins ?Page 7 of the schematic folio is very confusing.I just found pin 3 & 4 of the stmod+2 to be mapped to PG10 & P...
https://www.st.com/en/evaluation-tools/stm32f7508-dk.html is NRND'd.It's no huge loss, though, as it's an identical board (MB1911) to the 'F743 'F746 Disco (thanks, Clive!) which is still Active.JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.