2023-04-15 5:56 AM
2023-04-19 12:29 PM
Hello Manuel
The STMPE811QTR is an obsolete device and not available as a stand-alone device. The STM32F429I-DISC1 is available on the eStore but not the obsolete STMPE811QTR.
Best Regards
ST Support
Doug
2023-04-15 7:07 AM
The part is obsolete, so probably not going to be available in single quantity from retail distribution.
Check your return policy with your board vendor.
2023-04-15 7:28 AM
Thanks for reply!
I have bought it directly on https://estore.st.com/en/
ST still sell products, which use STMPE811QTR anyway (e.g. STM32F429I-DISC1) and stop availability and producing of spare parts, and they do not offer any compatible device regarding this component?
Have I understood that correctly?
2023-04-19 12:29 PM
Hello Manuel
The STMPE811QTR is an obsolete device and not available as a stand-alone device. The STM32F429I-DISC1 is available on the eStore but not the obsolete STMPE811QTR.
Best Regards
ST Support
Doug
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.