2023-07-12 3:05 PM - edited 2023-07-13 8:36 AM
I'm using a NUCLEO-H563ZI board with the onboard st-link, Cube IDE 1.12, on an intel mac running macos 13.4.1.
What I'm observing is that when I start a debug session is that if I set a breakpoint and hit continue i'll hit the breakpoint almost instantly, but if I click step-over it can take 10 or more seconds to hit the next line of code. I launched the st-link_gdbserver from the command line and used command line arm-none-eabi-gdb and had the same behavior. If I did `b main.c:80` and then continue i'd hit the line instantly, but if I hit `u` in gdb it could take 10 or more seconds to get to the next source line. It isn't always the same source lines, sometimes a line that took 10 seconds will be instantaneous the next time you try it.
I have a few coworkers reporting similar behavior. Any Ideas? The st-link reports a 8000KHz link speed. I'm not sure where the issue is in the chain.
I attached a video demonstrating the issue, sorry for the low quality I had to fit in the 5 MB limit :p .
Detailed version info:
CubeIDE: 1.12.1
arm-none-eabi-gdb : GNU gdb (GNU Arm Embedded Toolchain 10.3-2021.07) 10.2.90.20210621-git
STM32CubeProgrammer (STM32_Programmer_CLI) : 2.13.0
ST-LINK_gdbserver: 7.3.0
ST-LINK FW : V3J11M3
SWD freq : 8000 KHz
MacOS: 13.4.1 on an Intel
Solved! Go to Solution.
2023-07-14 9:25 AM
The problem has gone away if I use 12.X version of both GDB and GCC. No clear indication as to why but I hope this can help someone else.
2023-07-13 8:34 AM
I don't think this is the whole answer but there appears to be a correlation between having an issue if running arm-none-eabi-gdb version 10.X while version 12.X appears to not have the issue.
2023-07-14 9:25 AM
The problem has gone away if I use 12.X version of both GDB and GCC. No clear indication as to why but I hope this can help someone else.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.