2023-09-18 9:55 AM
Hi,
I sometimes get this error when starting a Debug on an F439ZI
Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (5) Unknown MCU found on target.
Unplugging and replugging the USB to the ST-link fixes it, but it is a bit perplexing. Is there a better way?
2023-09-18 10:27 AM - edited 2023-09-18 10:28 AM
Hello @alanb
I think that the problem come from the port usb in your PC or the cable you are using.
I suggest you to try to change them.
Best regards.
II
2023-09-19 7:12 PM
Going into low power modes or changing the function of SWDIO/SWCLK pins can cause debugger connection issues.
Are you using a counterfeit programmer? Is this a custom board?
2023-10-13 3:16 PM
No, I'm using a genuine Nucleo F439ZI board. But it was connected and powered from a laptop so it is I guess possible that the laptop USB didn't supply enough current. I have added an external power connector to my daughterboard.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.