STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Fast pin toggling on STMH723

I have been trying to see how fast can I toggle the pins on STM32H7 MCU. I'm using a nucleo-H723zg board. the clock configs are at the highest (550Mhz for CPU, 275 for APB and AHB), the pins are configured as very high speed. But still with a simple ...

Mazz by Associate II
  • 5893 Views
  • 11 replies
  • 3 kudos

Resolved! STM32F407G-DISC1 does not support virtual com, I cannot send data to PC via UART through virtual com

Hi All,I can not send data from the board to the PC via UART. I can see that USART2 can be used as virtual com. But, when send data from board to the PC, I can not see anything on serial port, I use TeraTerm, Putty, Hercules. I thought the new versio...

demir by Senior II
  • 8519 Views
  • 13 replies
  • 5 kudos

STM32 SD Card write multi block

Hello,I'm working on an STM32H7xx device. I'm trying to implement a system that writes data to a 'high capacity' SD Card. My goal is to be able to use the SD Card in a circular way. I'm having difficulty implementing this mechanism because I observe ...

Resolved! STM32 NUCLEO G071RBT6 Memory map

Hello everyone!I am looking for the memory map of the STM32 NUCLEO G071RBT6 board, specifically the addresses of the bootloader, application, and the size of the bootloader. I have tried searching for this information on various datasheets and websit...

Resolved! Error in Nucleo-U031R8 SCK Connection

I fear there is an error in the new Nucleo-U031R8 board. The D13 pin is labeled as the SPI1 SCK pin on the boards' silkscreen. However, the board schematic shows that this is connected to PA5. STM32CubeMX reports pin PA1 as the actual SPI1 SCK pin.So...

JSGraaf_0-1713917280613.png JSGraaf_0-1713917709786.png
JSGraaf by Associate III
  • 1798 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.