STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

nucleo pd output 24V@3A

Can I safely get that power out of any of the nucleo PD boards with a usb3 pd input? Can I get any higher current or voltage?  Output is 2 pin barrel connector. Target application is fully documented here. Thanks so much in advance Joe 

Resolved! HX711 LOAD CELL on STM32G0B1RCT6

HI,i am trying to interface the HX711 Load Cell to STM32G0B1RCT6 Microcontroller.i using internal clock source(HCLK = 16MHz) and  its reading good.Load Cell Value: 8220309Load Cell Value: 8221048Load Cell Value: 8221228Load Cell Value: 8221368Load Ce...

Can not detect USB Nucleo F411RE

Spoiler  My ST-Link was working perfectly at first. I could connect it to USB, upload code, and toggle the LED using a button. However, after upgrading the ST-Link firmware, my computer can't detect it via USB anymore. Any suggestions on how to fix t...

robotanh by Associate
  • 1196 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.