Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I'm using nucleo f446 board for adc sampling the internal adc is unidirectional. Is there any other development board like nucleo or discovery with internal ADC which can give both positive and negative cycle of adcPlease suggest me so that I can avo...
Hi,I have a STWIN.box , I would like to know how can I switch it off without unplugging the battery. It has a PWR button that works to switch it on but I can not find out how to switch it off.https://www.st.com/en/evaluation-tools/steval-stwinbx1.htm...
Hello guys, I want to control 128*64 GLCD(S6B0108) with STM32 blue pill. I searched many resources on the internet but I could't find any useful example.Any Examples?
I am mostly wondering if anyone here has ever had to code to communicate with a SSD1353 via stm32. I have used NHD documentation to connect the board in a 6800 Parallel interface. I know it is wired correctly as I connected it to my Arduino and used ...
Hi, Recently, I purchased a X-STM32MP-GNSS2 Evaluation board which came with an antenna. As per the instructions, I could find its compatibility with STM32MP157F-DK2 and Raspberry Pi. Can anybody help me getting its interface and data logging using ...
On STM32H747I-DISCO schematic, there are two different grounds. Why is SMPS ground connected to B6, C16 and T12?
I´m using a stm32f4 discovery board, and when i try to connect it to my computer it show "No ST-LINK detected". I don´t know if there are specials drivers for windows 11.
Good evening everyone,today I generated a sine wave (using array method, 80 samples per time period) and got it on oscilloscope using DAC channel 1. Then I tapped this analog wave into the ADC of the board. Then i again converted the data from ADC ch...
How can I enable Serial Wire View (SWV) on the STM32U031R8 controller? I am receiving a "tracing is not supported" pop-up window. Additionally, when I try to enable it from the debug configuration, the option appears to be disabled. Could this be bec...
Hello I can't able to connect my NUCLEO - H7A3ZI -Q. Its showing error while commenting.Please help me with solving this issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.