2025-10-28 3:10 AM
Hello ST Community team,
on the MB2046 schematic, there is a button called B3 or Boot mode pin:
But the UM3353 (chapter 7.9) mention only B1 and B2:
Could you please correct this on the coming doc revisions.
Best Regards.
II
Solved! Go to Solution.
2025-10-28 3:22 AM - edited 2025-10-30 12:31 AM
Hello @Issamos
Thank you for having reported this.
You are right ! The function for B3 Boot mode is missing description in UM3353.
An internal ticket ID 220601 is submitted in order to correct this.
(PS: Ticket ID 220601 is an internal tracking number and is not accessible or usable by customers).
2025-10-28 3:22 AM - edited 2025-10-30 12:31 AM
Hello @Issamos
Thank you for having reported this.
You are right ! The function for B3 Boot mode is missing description in UM3353.
An internal ticket ID 220601 is submitted in order to correct this.
(PS: Ticket ID 220601 is an internal tracking number and is not accessible or usable by customers).
2025-12-16 3:30 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.