2021-05-07 12:38 AM
I am using STLINK V3 with the ISOL board, and using the supplied 10-core cable, going to this connector in my 32F417 target
https://peter-ftp.co.uk/screenshots/202105072011602908.jpg
On the target connector, I have pins 3,5,7,9 grounded.
Pins 2,4,6,10 go to CPU pins PA13,PA14,PB3,PB4.
It works, but reliably only for code download. If I try to run SWV ITM data console, that also works but very soon I get a loss of comms. I am running at 8MHz; the ISOL debugger can go up to about 15MHz before it fails. I tried it at 1MHz but the same happened.
The wires to the CPU are pretty short - 5cm max.
I would be grateful for any ideas.
Console output:
------ Switching context -----
Target connection mode: Default
Reading ROM table for AP 0 @0xe00fffd0
Hardware watchpoint supported by the target
Failed to set com freq, status 0
COM frequency = 8000 kHz
ST-LINK Firmware version : V3J7M2B4S1
Device ID: 0x413
PC: 0x8025688
ST-LINK detects target voltage = 3.25 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
SWV_SetStatus(true): stop_reply_pending == 0
handle_vCont_c, continue thread
ST-LINK device status: RUN_MODE
ST-LINK device status: HALT_MODE
SWV_SetStatus(false): stop_reply_pending == 1
TraceCaptureStart and SWV event set to APP_FALSE (0)
NVIC_DFSR_REG = 0x0000000A
SWV_SetStatus(true): stop_reply_pending == 0
handle_vCont_c, continue thread
ST-LINK device status: RUN_MODE
ST-LINK device status: Failed to get status, Target not responding, retrying... 19
Target is not responding, retrying...
ST-LINK device status: Failed to get status, Target not responding, retrying... 19
Target is not responding, retrying...
ST-LINK device status: Failed to get status, Target not responding, retrying... 19
Target is not responding, retrying...
2021-05-07 6:17 AM
As usual, nobody answers.
Anyway, I solved it. There seems to be a fault on the MB1440B board, when stacked on top of the MB1599B board (the ISOL board). The 20-way connector works but the 14-way (CN1, which is used for the 10-way cable) does not. Well, it works but with a lot of intermittent faults. The solution is to not use MB1440B and plug the 10-way cable into the MB1599B board instead (CN1 also).
2021-05-28 10:20 AM
Hi @PHolt.1 ,
I added this thread to your post as contains the same topic, and this will help other users find that discussion faster.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.