2014-02-17 12:54 AM
hi ,
1.what is the page size in M24SR-16 ? in the datasheet its declared that write time for page in I2C = 5ms , write time for up to 264 bytes =150ms 2.Is it normal after writing 5 bytes to the M24SR , i am getting Frame extension of 2*9.6ms ?3.when authenticating using password in order to gain Read / Write Access , does it much time as writing 16 bytes ? #fwi #m24sr #i2c #m24sr #ndefSolved! Go to Solution.
2014-03-05 2:42 AM
Hello,
Please find here below answer to each point1. In Scenario 1,3 the R-APDU you got is 036A824F75 => SW1=6A SW2=82 ,which means ''File or Application Not Found'' (Table 24 Datasheet) , So the Write Process Didn't Start .
This mean the sequence applied was not correct .
Before to access or update a NDEF it is need to
s
elect correctly the application
Select correctly the file
Then you can access the file for reading or writing
2.In Scenario 2,4 the S-Block you got is F2020A72 , Which is Frame Extension request from the IC.
F2 service Instruction (waiting time extension , no DID)
02 WTX parameter
0A72 CRC
The M24SR calculate by itself the requested time extension parameter WTX in function of the Update request .
In your case WTX parameter is equal to “02�
The reader Must Acknowledge by sending the same service instruction thus in your case F202 0A72
After what the update will start .
2014-02-19 9:41 AM
°) 16 byte , but the M24SR is organized in file ,
So the write time is function of several parameters :
-
If we change or not the message Length (offset 00 but physically outside the user area) (1 programming time)
-
the number N of physical page supporting the message ( N * programming time)
-
and FWI = 9.6 ms authorizing only 1 Prog
Thus
1)
Change P1P2 : 1 prog , No extension
02-19-2014 16:33:16 NFC SEND I-Block
>>> CR95HFDLL_SENDRECV,
0300D6000002000BB889
08<<< 8008
036A824F75
0800002)
Change P1P2 : 1 prog + 1 byte , 2 Prog , Extension request -> Accept extension , Pog OK
02-19-2014 16:37:40 NFC SEND I-Block
>>> CR95HFDLL_SENDRECV,
0300D6000003000BD1F5E2
08<<< 8007
F2020A72
08000002-19-2014 16:37:40 NFC SEND SWTX_Block
>>> CR95HFDLL_SENDRECV,
F2020A72
08<<< 8008
0390002D53
0800003)
Change 14 byte , first row (except P1P2) 1 Prog , Pog OK
02-19-2014 16:31:51 NFC SEND I-Block
>>> CR95HFDLL_SENDRECV,
0200D600020ED1011F55017777772E73742E636FCE80
08<<< 8008
026A82932F
0800004)
Change 2 byte , first & second row 2 Prog , Extension request -> Accept extension , Pog OK
02-19-2014 16:40:53 NFC SEND I-Block
>>> CR95HFDLL_SENDRECV,
0200D6000F02636FE1D0
08<<< 8007
F2020A72
08000002-19-2014 16:40:53 NFC SEND SWTX_Block
>>> CR95HFDLL_SENDRECV,
F2020A72
08<<< 8008
029000F109
0800002°) For me the first extension occurs when programming on two page ,
Don’t forget to respond to a Service command “Waiting time Extension� request ie:
F2020A72
by the same Service command ie:
F2020A72
3°) Yes this is normal , purpose to prevent from hacking by increasing the command time ( there is none physical writing)
I hope this is clear enough, Best regards, ST NFC/RFID Dynamic support2014-02-23 2:55 AM
Thanks for the quick reply ,
1. In Scenario 1,3 the R-APDU you got is036A824F75
=> SW1=6A SW2=82 ,
which means ''File or Application Not Found'' (Table 24 Datasheet) , So the Write Process Didn't Start .
2.In Scenario 2,4
the S-Block you got is
F2020A72 ,
Which is Frame Extension request from the IC.
from what understand page size is 16 Bytes , but there are few exception :1.If i change the NDEF message length bytes , it will take 1 Prog time .2.The Number of Page I am crossing during Write , Number of Page *Prog time
If you can clarify your reply I really appreciate.2014-03-05 2:42 AM
Hello,
Please find here below answer to each point1. In Scenario 1,3 the R-APDU you got is 036A824F75 => SW1=6A SW2=82 ,which means ''File or Application Not Found'' (Table 24 Datasheet) , So the Write Process Didn't Start .
This mean the sequence applied was not correct .
Before to access or update a NDEF it is need to
s
elect correctly the application
Select correctly the file
Then you can access the file for reading or writing
2.In Scenario 2,4 the S-Block you got is F2020A72 , Which is Frame Extension request from the IC.
F2 service Instruction (waiting time extension , no DID)
02 WTX parameter
0A72 CRC
The M24SR calculate by itself the requested time extension parameter WTX in function of the Update request .
In your case WTX parameter is equal to “02�
The reader Must Acknowledge by sending the same service instruction thus in your case F202 0A72
After what the update will start .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.