2022-12-21 2:57 AM
Hardware:
Im using SP1 of the STM32L476RET:
SPI1_MOSI -> PA7
SPI1_MISO -> PA6
SPI1_SCK -> PA5
SPI_CS ->PB6
and Ext Interrupt:
IRQ_3911 -> PA0
my LEDs on:
LED_A -> PB0
LED_B -> PA4
LED_F -> PA1
LED_V -> PAB4
LED_AP2P -> PB5
LED_Tx -> PA8
Solved! Go to Solution.
2022-12-21 11:45 PM
Hi Titus,
I fail to grasp your question. Maybe (I didn't check) the connections are the same as for our ST25R3911B-DISCO, X-NUCLEO-NFC5 + NUCLEO-L476 then you can just use one of the existing examples.
If the connections are not the same you will need to port one of the demos - would recommend to start with ST25Embedded NFC lib as it is the most up-to-date one.
Ulysses
2022-12-21 11:45 PM
Hi Titus,
I fail to grasp your question. Maybe (I didn't check) the connections are the same as for our ST25R3911B-DISCO, X-NUCLEO-NFC5 + NUCLEO-L476 then you can just use one of the existing examples.
If the connections are not the same you will need to port one of the demos - would recommend to start with ST25Embedded NFC lib as it is the most up-to-date one.
Ulysses
2022-12-22 2:11 AM
2022-12-22 6:47 AM
Correct
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.