cancel
Showing results for 
Search instead for 
Did you mean: 

How to hand-make a ~15 cm loop antenna for STEVAL-25R200SA?

MelioNB
Associate II

Hi,

Follow-up to my earlier thread:
https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/st25r3911b-disco-for-rfid-mid-range-in-a-box-with-constraints/m-p/894801#M13962
where a similar hand-wound loop approach was discussed, I tried to reproduce it but it won't work. On the GUI I get a score of 2 on the RF field measurement.

I'm a real beginner in RF. I'm using the STEVAL-25R200SA and I want to build my own ~15 cm diameter loop antenna by hand for ISO 15693 tags.

What I've done so far: I wound a loop with enamelled copper wire, scraped the enamel off both ends to get a clean copper contact, and connected it on the Flexible Antenna daughterboard. Photo of my setup attached.

Is the flexible antenna the best route for a custom antenna, or should I use the 50 Ohm interface board instead?

Could someone give me a step-by-step on how to build and tune the loop myself (number of turns, geometry, target inductance, matching)?

Thanks!

2 REPLIES 2
AScha.3
Super User

Hi,

building an antenna is not difficult, but you have to measure, what you build.

So for 13.56 MHz - i suppose , you didnt tell frequency - you have to check, what you puzzle together.

A spectrum analyzer+tracking generator or a network analyzer is needed, maybe just a cheap one:

AScha3_0-1780848137698.png

- then you can check, what the antenna is doing:

AScha3_0-1780848729571.png

....where is the main resonance .

 

Without any measurement...its just rolling the dice.

 

btw

Your free flying wires to the box are a no go. At 13M your in the short wave radio range...and the rules of rf design apply.

AScha3_1-1780848342576.png

Here example from Ali , 13M, 

AScha3_0-1780850474359.png

34x40 mm ; 4 Wdg. -> about 0.7...1 uH.

so at 150 mm : 2 wdg. -> 1.3 uH --- too big.

minimum requirement is to get similar inductivity , and have connection wires short and close together, not wild flying.

try yourself, to get something around 0.9 .. 1 uH:

https://www.df7sx.de/luftspule/

.... 110 mm dia. + 2 Wdg. could work...try...

If you feel a post has answered your question, please click "Accept as Solution".
Brian TIDAL
ST Employee

Hi,

Informations about antenna design for ST25R200 can be found in Application Note AN6065 Antenna design for ST25R200 and ST25R100 devices.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.