2023-06-25 2:26 AM
2023-06-26 12:35 AM
Hi,
X-CUBE-NFC7 is dedicated to X-NUCLEO-NFC07A1 Dynamic NFC/RFID tag IC expansion board.
If your board is a X-NUCLEO-NFC05A1, you can use either the X-CUBE-NFC5 firmware package or the STSW-ST25R-LIB firmware package. I would recommand to use the STSW-ST25R-LIB. X-CUBE-NFC5 and STSW-ST25R-LIB both provide project files for STM32CubeIDE.
If your question is: "is X-CUBE-NFC5 supported in STM32CubeMX", the answer is no. As explained by Peter, this firmware package is not integrated in STM32CubeMX.
Rgds
BT
2023-06-25 11:45 AM
Welcome @FGang, to the community!
the ST25R3911B requires the use of X-NUCLEO-NFC05A1, which cannot be selected as an embedded software pack in the STM32CubeIDE because it was compiled several years ago and is therefore not compatible with the newer STM32CubeIDE. Instead, you can either open a project directly in its unpacked directory, or integrate the drivers (BSP, Middlewares) manually into your project.
Hope that helps?
Regards
/Peter
2023-06-26 12:35 AM
Hi,
X-CUBE-NFC7 is dedicated to X-NUCLEO-NFC07A1 Dynamic NFC/RFID tag IC expansion board.
If your board is a X-NUCLEO-NFC05A1, you can use either the X-CUBE-NFC5 firmware package or the STSW-ST25R-LIB firmware package. I would recommand to use the STSW-ST25R-LIB. X-CUBE-NFC5 and STSW-ST25R-LIB both provide project files for STM32CubeIDE.
If your question is: "is X-CUBE-NFC5 supported in STM32CubeMX", the answer is no. As explained by Peter, this firmware package is not integrated in STM32CubeMX.
Rgds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.