2025-03-15 12:23 AM
Hi Community,
I am designing an NFC card reader using a combination of the ST25R3916B NFC frontend and the STM32L476 MCU.
The ST25R3916B has four supply input pins:
In my setup, VDD_IO is powered by a 3.3V supply, while VDD_A, VDD_RF, and VDD_TX are powered by a 5V booster supply, as seen in the ST25R3916B-EMVCO reference schematic.
My question is: Is it okay or recommended to supply these three pins (VDD_A, VDD_RF, and VDD_TX) with 5V? I originally planned to power everything with a single 3.3V supply, but I noticed in the reference schematic that they are supplied with 5V. Would it make any difference if I powered these three pins with 3.3V instead of 5V? Reducing the number of supply voltages by using a 3.3V supply would make the design cheaper and eliminate the need for a booster IC, but would this negatively impact the NFC TX and RX performance?
Regards,
SB
Solved! Go to Solution.
2025-03-17 1:04 AM - edited 2025-03-21 1:47 AM
Hi SB,
please read DS chapter 4.2.10:
VDD_A is not to be supplied externally!
Putting VDD=VDD_TX=3V3 will reduce the achievable output power.
BR, Ulysses
2025-03-17 1:04 AM - edited 2025-03-21 1:47 AM
Hi SB,
please read DS chapter 4.2.10:
VDD_A is not to be supplied externally!
Putting VDD=VDD_TX=3V3 will reduce the achievable output power.
BR, Ulysses
2025-03-17 2:06 AM
Hi Ulysses,
Thanks for letting me know.
In the reference schematic, they have used a 5V supply for VDD and VDD_TX, while VDD_IO is powered at 3.3V for serial communication with the STM32L4.
I have one more question. They provided me with the schematic design of the reference board, but not the Altium design files.
If I want to use the same NFC antenna as the development board, how can I do that? Could you guide me on this? If the design files were available, I could replicate the same traces directly.
Best regards,
SB
2025-03-17 3:37 AM - edited 2025-03-17 3:41 AM
Hi SB,
which reference design are you looking at?
Previous post here: steval-st25r3916b-reader-expansion-board-circuit-schematic has Altium files...
BR, Ulysses
2025-03-17 4:35 AM
Hi Ulysses,
I am looking for this board's altium design files:
https://www.st.com/en/evaluation-tools/st25r3916b-emvco.html
Regards,
SB
2025-03-17 4:49 AM
Hi SB,
Sorry, we don't have the Altium project ready as sharable package.
BR, Ulysses
2025-03-17 8:08 AM
Hi Ulysses,
Did ST not develop Altium design files, or are they restricted due to an NDA or similar agreement?
If it's an NDA-related restriction, I will contact my sales manager to request access. However, if ST never developed these files, then there would be no point in reaching out to him.
I hope that makes sense.
Best regards,
SB
2025-03-18 2:54 AM
Hi SB,
Altium packages would need to be prepared (reviewed, cleaned). You can go through your sales manager to request them and receive then a lead time.
BR, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.