2025-03-16 7:53 AM
Hello everyone
I am creating an application on a PC that uses an ACR1552 reader and that must read and write to a ST25 device.
At the moment the data reading works and I am using the SDK of the reader manufacturer using the adpu commands.
I understand that in order to write to a previously protected area, I must enter the key (password) in order to then perform the writing operations.
I believe it is necessary to use an adpu mode called 'transparent' to be able to directly access the ST25 to write the password.
Although I have searched for some examples in the VBNET environment, I have not found anything.
Is there anything on this that can help me?
Thanks, Daniele
Solved! Go to Solution.
2025-03-19 3:11 AM
Hi,
I would suggest to contact the manufacturer of the ACR1552 reader in order to have the proper support.
Anyway, according to § "5.3.8. Accessing ISO15693 tags" in the user manual of the ACR1552, the Data part of APDU with Cla=FFh/INS=FBh/P1=00h/P2=00h is the non-addressed mode ISO15693 command being sent to the tag (without the SOF, without the request flags and without the EOF). I would just try to send the ST25DV password related command in the same way. E.g.for a Present Password command (B3h) with Password number=00h and Password = AA AA AA AA AA AA AA AA:
| Cla | INS | P0 | P1 | LC | Data | Le |
| FFh | FBh | 00h | 00h | 0Bh | B3 02 00 AA AA AA AA AA AA AA AA | --/00h |
Rgds
BT
2025-03-19 3:11 AM
Hi,
I would suggest to contact the manufacturer of the ACR1552 reader in order to have the proper support.
Anyway, according to § "5.3.8. Accessing ISO15693 tags" in the user manual of the ACR1552, the Data part of APDU with Cla=FFh/INS=FBh/P1=00h/P2=00h is the non-addressed mode ISO15693 command being sent to the tag (without the SOF, without the request flags and without the EOF). I would just try to send the ST25DV password related command in the same way. E.g.for a Present Password command (B3h) with Password number=00h and Password = AA AA AA AA AA AA AA AA:
| Cla | INS | P0 | P1 | LC | Data | Le |
| FFh | FBh | 00h | 00h | 0Bh | B3 02 00 AA AA AA AA AA AA AA AA | --/00h |
Rgds
BT
2025-03-19 3:52 AM
Dear Brian
Thanks for suggest, seems correct
Thanks again, Daniele
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.