2024-11-16 5:29 AM
Hi there,
first of all: I'm a software engineer and working with electronics only as a hobbyist. Therefore expect *** errors :)
I'm trying to use a ST25R3916B in my ESP32 project. The I2C communication to the ST25R3916B is working.
The call to rfalNfcInitialize succeeds but the next call to rfalFieldOnAndStartGT causes the ESP32 to crash with a " Core 1 panic'ed (Interrupt wdt timeout on CPU1).". The interrupt is taking too long.
Looking into the code, I found this function:
/*******************************************************************************/
void RfalRfST25R3916Class::st25r3916CheckForReceivedInterrupts(void)
{
uint8_t iregs[ST25R3916_INT_REGS_LEN];
uint32_t irqStatus;
/* Initialize iregs */
irqStatus = ST25R3916_IRQ_MASK_NONE;
ST_MEMSET(iregs, (int32_t)(ST25R3916_IRQ_MASK_ALL & 0xFFU), ST25R3916_INT_REGS_LEN);
/* In case the IRQ is Edge (not Level) triggered read IRQs until done */
while (digitalRead(int_pin) == HIGH) {
st25r3916ReadMultipleRegisters(ST25R3916_REG_IRQ_MAIN, iregs, ST25R3916_INT_REGS_LEN);
irqStatus |= (uint32_t)iregs[0];
irqStatus |= (uint32_t)iregs[1] << 8;
irqStatus |= (uint32_t)iregs[2] << 16;
irqStatus |= (uint32_t)iregs[3] << 24;
}
/* Forward all interrupts, even masked ones to application */
st25r3916interrupt.status |= irqStatus;
}
Commenting out the call to st25r3916ReadMultipleRegisters solves the crash but will also cause the interrupt to not work anymore (not a surprise).
This function is called by the interrupt and the call to st25r3916ReadMultipleRegisters does some I2C communication which (as far as I understand) should not be done in an interrupt handler.
Is this an incompatibility issue between the STM32duino ST25R3916 library and ESP32? Or am I doing something wrong? Has anyone gotten this IC to work on a ESP32?
Thanks for your time and your help :)
Solved! Go to Solution.
2024-11-18 2:54 PM
Thanks for the response. Increasing the watchdog timeout is probably not the best way to fix this. A function called by an interrupt should only run for a minimal time and should not do any complex task. I have moved the I2C handling outside the interrrupt function and now it works as expected.
Someone else has also observed the same issue and fixed it in this fork:
https://github.com/mcqn/ST25R3916
Additionally, I created my own fork https://github.com/rbuehlma/ST25R3916 based this one which fixes an issue when using I2C. It also allows to set the I2C address allowing multiple ICs to be used concurrently.
2024-11-18 1:03 AM
Hi,
"Interrupt wdt timeout on CPU1" means a watchdog timeout has occurred. I would suggest to increase the watchdog timeout.
What is the I2C speed? Using Fast Mode may also help
Rgds
BT
2024-11-18 2:54 PM
Thanks for the response. Increasing the watchdog timeout is probably not the best way to fix this. A function called by an interrupt should only run for a minimal time and should not do any complex task. I have moved the I2C handling outside the interrrupt function and now it works as expected.
Someone else has also observed the same issue and fixed it in this fork:
https://github.com/mcqn/ST25R3916
Additionally, I created my own fork https://github.com/rbuehlma/ST25R3916 based this one which fixes an issue when using I2C. It also allows to set the I2C address allowing multiple ICs to be used concurrently.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.