2025-05-21 11:15 PM - last edited on 2025-05-23 1:28 AM by Ulysses HERNIOSUS
st25r3911b in 14443A mode
TX: BITRATE_848
RX: BITRATE_1695
tx is successful,when receive , switch B mode , but fail :CRC error ,soft framing error and hard framing error
how can I solve this problem or Which registers still need to be modified?
Solved! Go to Solution.
2025-05-21 11:59 PM
Hi,
ST25R3911B supports only VHBR for ISO14443B. Although modulation scheme of A VHBR and B VHBR are the same, however the frame format is different (A VHBR having parity bits and CRC_A, where as B VHBR having start and stop bits and CRC_B).
I think you will not be able to succeed this way. Only if you would dive into transparent mode and let MCU do everything.
BR, Ulysses
2025-05-21 11:59 PM
Hi,
ST25R3911B supports only VHBR for ISO14443B. Although modulation scheme of A VHBR and B VHBR are the same, however the frame format is different (A VHBR having parity bits and CRC_A, where as B VHBR having start and stop bits and CRC_B).
I think you will not be able to succeed this way. Only if you would dive into transparent mode and let MCU do everything.
BR, Ulysses
2025-05-22 1:29 AM
I see,Thank you.
2025-05-22 4:06 AM
Hi,
to clarify this: VHBR is possible in B only. Tx in fc/8, fc/4, fc/2. Rx in fc/8 and fc/4. DS11793 rev7 is incorrect in this aspect.
BR, Ulysses
2025-05-22 6:14 PM
Thank you very much.
Are there any other RF chips that support VHBR in both modes A and B in reader mode?
Another question is that we have difficulties in waveform shaping when trimming the matching network of 3911 reader mode. There was a roughly 700mV overshoot in A waveform and very low modulation index in B waveform. We used the ST matching tool for the matching component value calculation. Do you have any suggestions for the further work.
Best Reagards.
2025-05-22 11:16 PM
Hi,
I am not aware of any other chips supporting VHBR. And especially none for A VHBR.
Waveshaping on ST25R3911B basically needs to be done through matching: Play with lower Q / play with different EMV inductors, ....
For modulation index you will need to adapt dram bits. Or use the direct command.
BR, Ulysses
2025-05-23 12:06 AM
I will try your suggestion. Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.