2025-06-17 5:03 PM
Hello,
I'm evaluating ST25DV for an application and am trying to characterize max available VEH voltage. I'm using STEVAL-SMARTAG1 board, and monitoring VEH output while enabling "Energy Harvesting" feature on the "NFC Tap" app. I can't seem to get above 3.4V on the VEH pin.
I've used both the embedded antenna, and as well as an external antenna (at which point I cut the embedded antenna traces). With the external antenna I made sure it is tuned to 13.56MHz while connected to ST25DV front end. I can confirm that the induced voltage is 9V (which seems to be due a clamping because when I disconnect the ST25DV I can get induced voltages well over 20V).
I'm trying to understand what is limiting VEH to 3.4V when I can clearly get quite a bit of voltage from the coil. The 3.4V limit seems to be also due to a clamp, because irrespective of the antenna position the voltage won't go above that, period. Once I move the antenna sufficiently far away, at some distance the VEH starts to quickly drop.
Is VEH indeed hard-limited to 3.4V internally, or am I missing a setting?
Solved! Go to Solution.
2025-08-27 2:15 AM
Hello,
Application note AN4913 "Energy harvesting delivery impact on ST25DV-I2C Series behaviour during RF
communication" gives a lot of infomations about Voltage and Current capability of energy harvesting pin as a function of the received field strength. It confirms the 3.4V limit you observe and most of the questions you may have.
Feel free to contact us for any further questions
best regards,
Henry Crane, NFC tag IC technical suport.
2025-08-27 2:15 AM
Hello,
Application note AN4913 "Energy harvesting delivery impact on ST25DV-I2C Series behaviour during RF
communication" gives a lot of infomations about Voltage and Current capability of energy harvesting pin as a function of the received field strength. It confirms the 3.4V limit you observe and most of the questions you may have.
Feel free to contact us for any further questions
best regards,
Henry Crane, NFC tag IC technical suport.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.